This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As per its functionality, if NOE is low ,Aport = Bport.
But when simulation is done ,the waveform is not as accepted, meaning Aport = Bport.
Kindly help to resolve this issue.
This is an old device designed for TTL signals that do not go near 5 V, so it uses a single N-channel transistor; see [FAQ] What are the Types of Architectures TI Switches and Multiplexers Use and how do I know which one my device has internally?
If you need to support signals up to VCC, use a switch with transmission gates, e.g., SN74HC4066 or TMUX1511.
Hey Ashwini,
Looks like you rejected this answer. Did you have any extra questions or thoughts here?
Can you maybe share what your inputs and outputs are and what you're using to simulate to help with our debugging and check is what you're seeing is expected?
Thanks
Rami