This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
Is the 240M bandwidth the -3dB bandwidth? If increasing the supply from 3.3V to 3.6V, would the bandwidth increase or decrease?
Thanks.
Yes; this is an analog switch, and the specified bandwidth is for the −3 dB attenuation of a sine wave. See figure 6-11 of the datasheet:
Increasing the supply voltage will increase the bandwidth by a very small amount.
Hi Di,
Clemens is correct here. 240 MHz is the -3dB bandwidth of the device. Increasing the supply would slightly decrease the bandwidth, but I recommend running the device through simulations to get a precise number if that is a key parameter.
Thanks!
Alex