Hello Team,
We have a problem that the compliance test can't pass due to not enough voltage amplitude. Test results are around ± 680mV against the regulation between ±950mV and 1050mV.
Our design is show below:
The voltage value at the input of the switches is about 2.5V but only one pin voltage value is 1.2V. How can I tell if it's before or after entering MUX? What could be the reasons for the low output voltage value?
Thank you in advance for your advise.
Best Regards,