what is the basic output structure of SN74CBTLV3245APWR?Does this switch require an external pull resistor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what is the basic output structure of SN74CBTLV3245APWR?Does this switch require an external pull resistor?
Is the following figure its output structure? Can I add an external pull-up/down resistor to a connected PIN ? Does the external pull-down resistor on the connected pin affect its function?

Hey hanbo,
yes, this is the internal architecture of the device. For information on the transmission gates we have an FAQ here :
Regardless of the architecture, this device, along with all our other analog muxes, act as passive components. So as Clemens mentioned "When a pin is disconnected, it is floating unless you add a pull-up/-down resistor".
So the external pulldown will effect the function of the output of the device, as it will pulldown the output.
Thanks,
Rami