This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3126: Bus switch application

Part Number: SN74CBTLV3126
Other Parts Discussed in Thread: TS3DDR4000

Hi,

Does TI have below bus swithc for below application?

I have searched on TI website seems but can't found VCC can support 1.2V. Thanks.

1、3600MT/s up throughput

2、12bit or 14-bit bus width

3、VCCQ : 1.2V

Jeff

  • Hello Jeff,

    The  TS3DDR4000 looks to be the best device for your application.

    1.It can support the 3600MT/s which in DDR applications mean 1800MHZ signals. This is because its bandwidth is  6 GHZ(6000MHZ). Check out this FAQ to learn more.

    2. This device is a 2:1 12 channel( bit) device. The device can be used like a 1:1  12 channel mux  using the control logic table in the datasheet. Our team recommends the unused io pins be terminated to ground through 50 ohm resistors in high speed applications like this . For more info on this please read this FAQ.

    3.Finally, this device does not have a VCCQ pin(output stage logic power voltage), instead all of the device's internal circuitry power supply is the VDD pin.

    Please let me know if this device what you think about this device and I can answer any follow up questions!

    regards,

    Kameron

  • Hello,

    Any update on this!

  • Hi Kameron,

    Sorry for forgot reply this. I have suggest TS3DDR4000 to customer. And they also have used this chip in old design.

    Thanks!

    Jeff