Hello,
I'm working on an analog design where we measure small time intervals (on the order of tenths of nanoseconds). We use the standard technique of starting/stopping a current pump, which linearly charges a precision capacitor. So far so good, we are getting good precision and resolution. We are evaluating different analog switches, from the humble 74AUC1G66 (which works great!), to the TMUX1101 and others.
My question is, what is the aperture jitter of these switches between the control signal transition and the actual action of the switch? Can you give a rough estimate/order of magnitude?
Our hypothesis is that the aperture jitter (uncertainty) may be a fraction of the enable/disable time. According to this, the faster to enable/disable 74AUC1G66 (around 1ns) should have a lower aperture jitter than the, for instance, TMUX1101 (9-17 ns).
Any information you can share is more than welcome!
Regards,
Jose Jimenez