This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1574: Questions about the operation of TMUX1574DYYR

Part Number: TMUX1574

Tool/software:

Hi,

Could you please tell me two points about TMUX1574DYYR?

(1) What is the operation at the moment of switching from A to B or B to A by the SEL pin?
 Which operation is the OUTPUT connected to either AB or not connected to either AB?

(2) If the voltage of the EN pin is less than the High threshold, is it correct to say that the OUTPUT is not connected to either AB or B?

Regards, Takumi