Other Parts Discussed in Thread: TMUX6234
Tool/software:
As mentioned in the related post, the PSpice model for the TMUX7234 is faulty and the following Error is thrown:
There is a bugfix-model provided in the related post, which is not yet updated in the library.
If I use this model and add it to the library path, PSpice switches into the "Third-party-parts-included"-mode and supports only 3 probing points.
When will the model in the library be updated, to avoid this problem?
Is there a possibilty to include the library on a way, PSpice detects that this bugfix-model is provided by TI?
Thanks,
Milan