Other Parts Discussed in Thread: TSC2007, TPS22919, TPS22995
Tool/software:
This IC is used as the POR for TSC2007. The circuit is as shown below.
If no resistor is inserted between pin-D and the load, an inrush current of 3.3V / Ron will flow each time the SW is switched.
Since Ron(min) = 4.5Ω, a peak current of 3.3/4.5 = 0.74A will flow.
Will this value damage the IC?
The TSC2007's Vdd fall speed is 2kV/s~. The rise speed is 12kV/s~, so I do not want to insert a resistor.