This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Ti
Is the TMUX1574 suited for differential signals like SGMII ?
From the datasheet it seems to be only applicable to single-ended applications?
Regards
Piet
Hi Clemens
Is the skew between the channels low enough to produce a good eye opening for a differential signal at the maximum bandwidth of 2GHz supported by the device?