This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX4157N: The questions of design using TMUX4157N

Part Number: TMUX4157N


Tool/software:

Dear TI :

We will use TMUX4157N to design our product.
The signals of VSS and S2 are connected to -5V. The signal of S1 is connected to GND.
Use the signal of SEL to select the output :  -5V or GND.

Question 1 : Is it the correct the design?
Question 2 : Does the large current loading influence the output voltage ?

Thanks