Tool/software:
Hi Team,
I am using TMUX1574RSVR for the SPI MUX in my design, where 2 master SPI will be connected to source side of MUX chip & Drain side will be connected to SPI flash.
while doing DC analysis, there is no VIH, VIL and VOH, VOL values for the Source & drain pins of the TMUX1574RSVR datasheet.
one of the 2 master's is failing in the DC,
1.(Master) SOC which has VOH=2.475, VOL=0.825, when i consider the MUX has only FET with Rdson of 4ohm (max) with 0.1mV drop bypassing the MUX and comparing the source side and drain side connected device directly with 0.1V drop.
also even if i did not consider the MUX voltage drop in DC analysis, the source side Device & Drain side device is failing in DC for low levels. when we use MUX, do we have better VOL, VIL from MUX, so that DC levels will be met?
How to get the VIH, VIL, VOH, VOL values of the TMUX1574RSVR.