Tool/software:
Hi team,
we are using TMUX1574RSVR in our project. we are facing issue when we transmit SPI signals through that part.
Issue:
we are transmitting SPI signals with clock frequency of 125khz with the voltage level as 5V,
while doing so we observed that the SPI signals are not as expected. while probing the signals at both ends we found out that my input signals is as expected but, my output at bank A is not as expected. upon further investigation we found out signals from pin 3 (miso) is always Low. we checked slave device and its works fine.
hence we replaced the MUX. Even after mux replacement we are facing issue in bank B (8th pin) is always low and the Bank A signals are now as expected.
Kindly confirm the cause for it and please suggest us to take care if suppose this error reappears.
Thanks and regards
Venish S