This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Application team:
We would like use SN3257-Q1 design for standard I2C 2:1 switch control as like application.
Could you please help review the design can workable for Standard I2C(100k /400k) switch selection? is any rising /falling spec can meet I2C protocol or not? thank you
Hello Clemens:
Yes, could you advise smaller and cheaper solutions for our reference?
(1)Do you need to switch two or four signals? -> Could you share all solutions we can choose which is suitable for our design ?
(2) At what voltage ? -> 1.8V to 3.3V .
(3) Need Automotive grade solutions
Roy