This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello community,
I'm a little bit confused about the datasheets (e.g. TS3A44159) for your analog switches.
Most of them are defined with:
"Analog voltage range -0.5V ... V+ + 0.5 V"
So I've got an Audio Signal, which is sinusoidal wave +-1.5V.
And also in the application notes there are examples with Audio sources.
Are These switches able to switch such audio signals?
Thanks in advance
Michael