This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using CD4097B as an 8-way USB 2.0 Multiplexer

Other Parts Discussed in Thread: CD4097B, TS3USB3000, TS3DS10224, SN74CB3Q3251

Hi,

I'm trying to use the CD4097B(PWR) as a 1:8 USB 2.0 multiplexer. Even though it's a differential multiplexer, it doesn't seem to work. Is it even possible with this chip, or are the USB D+ and D- signal too low voltage for this chip to work properly as a USB multiplexer? Could any one provide me any reference designs as to how this would work (Currently I'm doing this on a breadboard; maybe that's my issue). Also, are there any other chips capable of doing 1:8 USB 2.0 (without cascading). I'm looking for a TI chip similar to the MAX4999.

I appreciate your help.

Thank you and best regards,
Ali

  • Ali,

    The CD4097B does not have enough bandwidth to support USB 2.0 signals. You would need to look at the TS3USB3000 TSeUSBXXXX family of switches to support USB 2.0 applications.

    I couldn't find a device equivalent to the the MAX4999. The closest match to an 1:8 USB 2.0 mux is the TS3DS10224 that can be configured as a 1:4 USB mux. You would need to use 2x TS3DS10224 devices.

    Thank you,
    Adam
  • That would explain a lot. What kind of bandwidth would be required to support USB 2.0? Also, is there a reference design for using TS3DS10224 as a USB 2.0 1:4 Mux?

    Thank you for your help.

    Best regards,
    Ali
  • Ali,

    Please see the FAQ thread question number 2 for the answer to what kind of bandwidth would be required to support USB2.0.  The USB 2.0 standard states max data rate of 480Mbs so ~720MHz is need.

    https://e2e.ti.com/support/interface/etc_interface/f/388/t/437256

    We are in the middle of updating the datasheet.  Here is a preview of how to configure the device for 1:4 mux

    Let me know if this helps.

    Thank you,

    Adam

  • Hi Adam,

    Thanks for this. However, I had looked at the datasheet and understood how it works. My question was more regarding a hardware reference design, like do I need to add any capacitors, or resistors, etc. of a specific value to specific pins when I'm actually implementing the circuitry for testing or can I do direct digital connections to all of the signal and control lines? Also, for doing a 1:8 using this chip, would it be as simple as branching the USB signals in to INA (or INB) of both chips.

    Thank you for your help.

    Best regards,
    Ali

  • Hi Ali ,

    SN74CB3Q3251 is 1:8 Mux which is suitable for USB 2.0 Multiplexing which could be considered as well .
  • Thank you Shreyas. I've ordered some samples, I'll test it out to see if it works.

    Best regards,
    Ali
  • Would either of you know if CD74HC4351E would work?

    Thanks,
    Ali
  • Although it is 1:8 Mux , it is bandwidth limited to 180Mhz.
  • Ali,

    The signal switches do not require any external components to operate so we do not have any reference schematics available. We do recommend placing a bypass capacitor on the supply pins as good practice.

    Yes a two IC solution using the TS3DS10224 as a 1:8 mux would be connecting your USB 2.0 PHY to an input of each IC and then use the GPIOs and truth table to mux the signal accordingly.

    Thank you,
    Adam
  • Shreyas,

    Thank you for the recommendation of other 1:8 mux. My one concern with using the SN74CB3Q3251 is that is not a differential switch. You would still need to have a two IC solution for using one IC for the D+ signal and one for the D-. Do you see any signal integrity issues having the D+ and D- signals going through two different ICs?

    Adam