This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need help interpreting the TS5USBA224 (integrated USB 2.0 and analog audio switch) datasheet.
1) Audio Switch:
Oiso=-83dB, it means the effect of USB D+/D- signal on the audio channel when USB communication is ongoing. Right?
Xtalk=-83dB here means the crosstalk between left and right channel?
Both specs are taken at 20kHz frequency point?
2) USB Switch:
Oiso=-22dB, it means the effect of Audio L/R signal on the USB channel when audio signal is on transferring. Right?
Xtalk=-21dB here means the crosstalk between D+ and D- channel?
Both specs are taken at 240kHz frequency point?
3) When chip is operating, does D+/R pin output DC level? How much the value?
4) When audio input via USB connector, need insert coupler capacitor between D+/R pin and audio source?
From datasheet, VR, VL range, there should be DC at D+/R pin.
5) From internal block, this switch doesn't have an internal charge pump, will not support a signal swing over the supply voltage, so that means D+/R pin can only be positive signal. Right?
Ranita,
The TS5USBA224 is a passive, bi-directional, FET switch. This device is designed to select two different signals and simply pass the signal from one side of the switch to the other without degrading signal integrity. If you were to have an ideal model of the signal path it would be a 0 ohm wire.
1) Audio Switch:
Oiso=-83dB, it means the effect of USB D+/D- signal on the audio channel when USB communication is ongoing. Right?
Xtalk=-83dB here means the crosstalk between left and right channel?
Both specs are taken at 20kHz frequency point?
You can see the descriptions of how the parameters are measured in the parameter measurement section in the datasheet. The Oiso measurement is off isolation which describes the IC's ability to isolate the signal path when it is not selected. For example if there is a signal on the D+ and the audio path is selected this measurement describes how well the IC isolates the D+ signal from the D+/R path.
The Xtalk measurement does mean how much of the signal gets coupled onto an adjacent channel. We know there is an error in the datasheet that the audio path cross talk measurement is not taken over the audio band. We just designed hardware to take this measurement again and should have a revised version of the datasheet in a couple weeks.
2) USB Switch:
Oiso=-22dB, it means the effect of Audio L/R signal on the USB channel when audio signal is on transferring. Right?
Xtalk=-21dB here means the crosstalk between D+ and D- channel?
Both specs are taken at 240kHz frequency point?
The off isolation Oiso spec means the amount of signal passing through the switch from the unselected channel.
The cross talk spec describes the amount of signal coupling onto the adjacent channel either L/R pins or D+/D-.
3) When chip is operating, does D+/R pin output DC level? How much the value?
This is a passive device there the TS5USBA224 does not provide any DC output. If you require a DC offset in your system you will need to provide it externally to the switch IC.
4) When audio input via USB connector, need insert coupler capacitor between D+/R pin and audio source?
This will depend on the system requirements of your audio codec. The TS5AUSB224 device does not require any external components. The only design requirement is that the signals on the device must be within the recommend operating conditions.
I you would like to a reference design of using audio signals through the USB type C connect you can take a look at the materials in this post.
USB Type C audio: Do I need to buy a new pair of headphones? - Switches & multiplexers forum - Switches...
From datasheet, VR, VL range, there should be DC at D+/R pin.
Voltage on the L and R pins of the TS5USBA224 device can range from Vaudio (IC supply voltage) to Vaudio-5.5V. For example if your Vaudio (supply voltage) is running off of a 3.3 V rail you may have a signal on the L R and D+/R pins from -2.2 V to 3.3V. Most audio codecs have an out that is AC coupled so the audio signals are centered around 0V. This device is designed to handle the negative signals.
5) From internal block, this switch doesn't have an internal charge pump, will not support a signal swing over the supply voltage, so that means D+/R pin can only be positive signal. Right?
That is correct. The TS5USBA224 does not have an internal charge pump. The TS5USBA224 device can handle the negative signaling because it uses a transmission gate.
Here is a related post on the negative signaling.
TS5USBA224 Signal output relation to Vaudio - Switches & multiplexers forum - Switches & multiplexers...
Thank you,
Adam