This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Do we have solution have hot insertion sames as PI3C3384 ? Thank you.
BR
Patrick
Patrick,
I used the switches and multiplexers quick search tool to find several parts similar to the PI3C3384 even some pin to pin.
I searched 10 channel 1:1 SPST switches with the additional feature IOFF. IOFF feature is stating that the device is High impedance with Vcc = 0 V. I think this is what you mean by "hot insertion"
Quick search tool
The SN74CBT3384C is p2p with the PI3C3384 device.
Thank you,
Adam
Patrick,
What is the meaning of "hot swap"? The SN74CBTLV3384 can have a voltage present on the signal path without a voltage on the supply pin without damage. The signal switch path will be Hi-Z if there is no voltage on the supply pin.
Adam