This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kouki,
The range of the TPS22959 is 0A-15A, so even a small amount of current (such as 70uA) can pass through it when turned on.
Thanks,
Alek Kaknevicius
Hi Kouki,
That is correct. If the ON pin is high, then the FET is on (closed) and if the ON pin is low, then the FET is off (open).
Thanks,
Alek Kaknevicius