Hello Team
My customer have some issue about CD4051. Detail information, please see attached. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team
My customer have some issue about CD4051. Detail information, please see attached. Thanks.
Xiao,
How many parts do you have that are showing this behavior out of how many built?
I will wait for the schematic to see if there is anything that can cause an increase in DC offset voltage. Typically when a signal switch is damaged the symptom is lower voltages due to excess leakage in the part. I've never seen a signal switch increase the voltage.
Are you able to test the suspect unit for damage? A quick way to do this will be to power up the device, place a DC signal on the signal paths, toggle the switch with the control logic, and observe any high current through the pins. If placing a new part on the board solves the issue and placing the suspect part on a good board causes issue we may want to start getting ready to submit it for return.
Thank you,
Adam
New Microsoft Word Document.docxhello Adam
Sorry for late reply. I also test it in customer board. and update some new information . The output signal offset changed high, but the amplitude change small. It seemed there have a weak pull up to power.
Xiao,
This sounds like the part might be damaged as mentioned above.
If you remove the part from the customer's board and test it by itself, what is the leakage current you see going into the pin you think has a weak pull up to supply?
You can test the leakage by placing Vdd at 18V and set the logic control pins to turn on the suspect signal path. Then you can place a DC 18V on the suspect pin and measure the current flowing through that pin to see if it is within the spec.
Thank you,
Adam