This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A22364: Single signal input, NC2 is not used, float or connect to the GND ?

Part Number: TS5A22364

Dear team,

My customer wants to use single-ended input, so they only use NC1, don't use NC2. How do they deal with NC2, float or connected to the GND?

Thanks & Best Regards,

Sherry

  • Hi, Sherry,

    As mentioned in the FAQ section of the E2E post:


    What should I do with unused inputs/outputs of a switch?

    Switch channel inputs can either be left floating or terminated to GND (which can help reduce signal reflections). However, switch logic inputs, such as Select pins, OE pins, and other logic inputs, should never be left floating. They should  be, by default, tied to either VCC or GND.

    Regards,
    David