This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
My customer use TS3A227E for their headphone detecting. We meet question for defining standard and OMTP headphone:
1. We often monitor "standard" 4-pole headset in customer board or EVM. Any reason we can detect OMTP headset? Register or HW setting we have to take care?
2. We can't access EVM in some NB... any driver need to install the GUI?
Thanks for your kindly help.
Hi Gary,
1: This e2e post gives some more information on how TI's audio jack switches detect the difference between different types of headsets.
Does TS3A226AE support high impendance microphone (like IPhone 6 earphone ) ? (this post also explains...
Below register map table from the datasheet may help you with setting up OMTP mode
2: The EVM GUI is available here on ti.com.
Do you have Jumper J2 installed to connect Vcc to VDD and power the TS3A227E?
Thanks
Saminah
Hi Saminah,
We test some headsets by using evm and get the result as below:
1. Do you think the test result is currect? Do you think any evm setting issue in my test?
2. Do I have to reset the result on GUI by reading all register again or do any setting?
3. Is there limitation for TS3A227 in 4 role headset detection?
Thanks for your support.
Gary
Hi Gary,
can you upload the test result again - somehow it is not showing up correctly in e2e thread.
there should not be any issue with TS3A227 in 4 role headset detection - Once I review your test result, I can help you out better.
Thanks
Saminah
Hi Saminah,
FYI.
TI headset | samsung | asus | i6 headset | noname | |
r2 (ohm) | 32.7 | 31 | 32 | 42 | O/L |
rsleeve (ohm) | 5.42k | O/L | 2.5k | 649k | O/L |
G/M (ohm) | 5.4K | O/L | 2.48k | 645k | 700 |
debounce time = 7 | standard | standard | standard | standard | 3 pole |
debounce time = 3 | standard | 3 pole | standard / OMTP | standard | 3 pole |
debounce time = 4 | standard | 3 pole (most) | OMTP (most) | standard | 3 pole |
iphone 6 | Y | NA | NA | Y | Y |
Lenovo nb | Y | Y | Y | Y | Y |