This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Would you please help review the TS3A227E schematic and provide your comment?
BR,
SHH
SHH,
My main concern is note 12 with the DET_TRIGGER pin. The current schematic has opposite operation. You can place an inverter in between the phone jack switch and the DET_TRIGGER pin or choose a phone jack with the switch with the opposite operation.
1. VDD is correctly supplied with 3.3 V which is within the recommended operating conditions and includes bypass capacitors.
2. SCL and SDA are not used correctly tied to VDD
3. MIC_PRESENT is open drain output is correctly pulled up with a resistor.
4. MIC_P correctly connected to codec
5. INT# is not used and correctly connected to ground
6. GNDA for FM support features not used and correctly grounded
7. GND_SENSE is not used and correctly connected to ground
8. GND correctly connected to ground
9. SLEEVE and SLEEVE_SENSE correctly connected to sleeve of the phone jack
10. RING2 and RING2_SENSE correctly connected to Ring 2 of phone jack
11. Tip pin is correctly connected to the tip of the phone jack.
12. DET_TRIGGER pin to initiate the automatic detection sequence is not connected correctly. The phone jack looks like it has a normally closed switch that is connected to ground. This connection will pull the DET_TRIGGER pin low when no headset is in the phone jack. When the headset is insterted into the phone jack the phone jack switch will open and the DET_TRIGGER pin will go high due to the internal pull up of the TS3A227E. This operation is opposite of the required operation stated in the datasheet.
Thank you,
Adam