If the IN Drops below the min. Vcc level while the switch is active (com. connected to “Normally open"), will the switch disengage? (com. connected to "normally closed")
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the IN Drops below the min. Vcc level while the switch is active (com. connected to “Normally open"), will the switch disengage? (com. connected to "normally closed")
Hi Lauren,
How are you driving the "IN" pin and what is your supply voltage?
If IN is high, COM is connected to NO.
With a 5 V on the supply pin the minimum voltage on the digital input IN pin that the device will recognize as a logic "high" is 2.4 V.
With supplies 4.5 V or below on the supply pin the minimum voltage on the digital input IN pin that the device will recognize as a logic "high" is 2 V.
Regards
Saminah
Hi Saminah,
OK, so say the voltage dropped below the minimum level required to be considered a logic high (which you said is 2V). So say it drops to 1.5V or so. Will the switch disengage and connect to normally closed?
Hi Lauren,,
CMOS logic devices depend on their inputs being at either a logic HIGH or a logic LOW.
For 4.5V supply or below, To guarantee a logic low (VIL) the max voltage is 0.8V to connect NC to COM, and to connect NO to COM , the MIN voltage for logic High is 2V.
When the input is 'somewhere in the middle,' then both MOSFETs on the input can be turned on, which can cause a significant amount of shoot-through current. It is best to transition through this voltage region as quickly as possible to prevent shoot-through current. See FAQ here.
Check out the link to the TI Precision lab video that explains the logic levels in more details and details in this application report for Preventing Excess Current Consumption on Analog Switches.
Thanks
Saminah
Hi Saminah,
So it *won't* disengage, but it'll cause shoot-through. Got it.
Thank you!
Lauren
Hi Lauren,
Yes, to simplify it, the switch will be in "unknown" state when the Control signal is operating in the undefined region between VIL and VIH that can result in issues (like shoot-through current) related to slow changing across the threshold voltage.
TI application report on “Slow or floating CMOS Inputs” has detail explanation of the impact this can have on device performance.
Regards
Saminah