Hi,
We are using the SN74CBTLV3861 10bit bus switch to isolate our MCU pins from external loads as part of board power-up sequence.
One thing we have recently noticed is that the
We are operating from Vcc=3.3V
Case 1 (switch HighZ): A1 = open; B1 = pulled-up to 3.3V via 2kR; !OE=high .... then B1 measured reports 3.3V; A1 reports floating
Case 2(switch ON): A1=open; B1=pulled-up to 3.3V via 2kR; !OE=low...then B1 is measured as 3.15V; A1 reported 3.15V
For some reason the bus switch activation is causing the level on B1 to drop from 3.3V to 3.15V. We have noticed this on multiple parts and boards, so damage is unlikely.
Can you help us understand why the voltage drop in Case2 is occuring, even through the datasheet specified 5Ohm pass resistance and rail-to-rail performance?
FYI: the application for these pins is I2C (100k/400kbit/s) .
Many thanks!
Simon M.
to isolate