This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have tried to change Code Generation Tools for Sitara from V5.0.5 to V5.2.5. At the end of the rebuild the linker fails because Runtime Library "rtsv7A8_A_le_n_v3_eabi.lib" could not be found. So we have tried with V5.2.7 and V15.12.1.LTS which resulted in the same Problem. When I Switch back to V5.0.5 I can do a complete rebuild even after I have manually deleted the Runtime Library first.
I have read some other E2E posts addressing similar problems but without finding a solution to the problem. Some E2E Posts addressing problems that the build of the runtime library fails. But here the build does not even start.
Any help is appreciated.
Best regards,
Patrick
We recently discovered that when using the parallel builds feature of CCS, the automatic RTS library build may fail. So make sure you are not doing that. I suspect that is is already the case, and this is not the cause of your problem.
I am not aware of any other issues with automatic builds in compiler versions 5.2.7 or 15.12.1.LTS. Please copy-n-paste into your next post the invocation of the linker and everything that happens after that. Please see if some of the troubleshooting techniques discussed here are helpful.
In the meantime, you can manually build the RTS library you need. Here is how to do that.
Thanks and regards,
-George
George,
This is the output of the linker invocation:
'Building target: Project.out'
'Invoking: ARM Linker'
"C:/CCStudio_V6/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7A8 --code_state=32 --float_support=VFPv3 -me -O3 --opt_for_speed=4 --gcc --define=am335x --
diag_warning=225 --display_error_number --gen_func_subsections=on --neon --abi=eabi --opt_for_cache -z -m"Project.map" -i"C:/CCStudio_V6/ccsv6/tools/compiler/ti-cgt-
arm_15.12.1.LTS/lib" -i"C:/CCStudio_V6/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --reread_libs --display_error_number --warn_sections --
xml_link_info="Project_linkInfo.xml" --rom_model -o "Project.out"
<...All the projects object files...>
-l../AM335x_RAM.cmd -l"rtsv7A8_A_le_n_v3_eabi.lib"
<Linking>
error #10008-D: cannot find file "rtsv7A8_A_le_n_v3_eabi.lib"
undefined first referenced
symbol in file
--------- ----------------
__STACK_END ./AM335x_CodeStart.obj
__TI_auto_init ./AM335x_CodeStart.obj
__TI_decompress_none
__TI_decompress_rle24
__aeabi_idivmod ./xxxx.obj
__aeabi_uidivmod ./yyyy.obj
free ./zzzz.obj
malloc ./aaaa.obj
memcpy ./bbbb.obj
memset ./qqqq.obj
sprintf ./vvvv.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Project.out" not built
>> Compilation failure
gmake: *** [Project.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
The linker does not invoke automatic library build although the library does not exist.
So I have tried a TI example project from StarterWare. To my surprise the library gets built automatically:
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/demo/Release/demo.out'
'Invoking: ARM Linker'
<Linking>
warning: automatic library build: using library
"C:\CCStudio_V6\ccsv6\tools\compiler\ti-cgt-arm_15.12.1.LTS\lib\rtsv7A8_A_le
_n_eabi.lib" for the first time, so it must be built. This may take a few
minutes.
"../demo.cmd", line 89: warning: No placement specified for ".bss"; a default
placement will be applied.
'Finished building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/demo/Release/demo.out'
' '
' '
**** Build Finished ****
The difference is that this example project uses <automatic> in the CCS General settings under "Runtime support library" and I use "rtsv7A8_A_le_n_v3_eabi.lib". If I change the TI example to "rtsv7A8_A_le_n_eabi.lib" instead of "<automatic>" then it does not work as well:
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/demo/Release/demo.out'
'Invoking: ARM Linker'
<Linking>
error: cannot find file "rtsv7A8_A_le_n_eabi.lib"
"../demo.cmd", line 89: warning: No placement specified for ".bss"; a default
placement will be applied.
undefined first referenced
symbol in file
--------- ----------------
__STACK_END ../../../../../../../binary/armv7a/cgt_ccs/am335x/system_config/Release/system.lib<init.obj>
__TI_auto_init ../../../../../../../binary/armv7a/cgt_ccs/am335x/system_config/Release/system.lib<init.obj>
__aeabi_idivmod ./lwiplib.obj
__aeabi_uidivmod ./demoGrlib.obj
memcpy ./cm3wkup_proxy.obj
>> Compilation failure
memset ./demoRtc.obj
strcat ./demoMain.obj
strchr ./httpd_io.obj
strcmp ./demoEnet.obj
strlen ./httpd_io.obj
strncmp ./httpd_io.obj
error: unresolved symbols remain
error: errors encountered during linking;
"../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/demo/Release/
demo.out" not built
gmake: *** [../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/demo/Release/demo.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Now you could say "just use <automatic>". But we want to define what the linker has to use and it worked like this in the Code Generation Tools V5.0.5.
Any other suggestions?
Best regards,
Patrick
As an extension to my last post: It looks like Code Generation Tools V15.12.1.LTS do not behave as described in processors.wiki.ti.com/.../Mklib
As a special case, the linker will assume that if the requested library name matches one indexed by libc.a, then it really is the standard compiler RTS library with that name, and will proceed to build it. For this to be safe, users should not re-use the names of standard libraries for custom-built libraries.
I cannot reproduce that exact failure, but I can reproduce one that is very similar. I filed SDSCM00052868 in the SDOWP system to have it investigated. You are welcome to follow it with the SDOWP link below in my signature.
As another troubleshooting tip, please consider trying out this technique.
Thanks and regards,
-George
George,
I have checked my PATH variable as shown in Mklib article. There is no path pointing to an sh.exe, gmake.exe or cygwin.exe. I have to point out that with ARM CGT V5.0.5 everything works as expected. ARM CGT V5.2.7 and ARM CGT V15.12.1.LTS does not work as expected.
I use CCS V6.1.1.00022 on a Windows 7 32Bit OS. Attached is an Excel file with the installation details.
Best regards,
Patrick