Hi,
We have tried to change Code Generation Tools for Sitara from V5.0.5 to V5.2.5. At the end of the rebuild the linker fails because Runtime Library "rtsv7A8_A_le_n_v3_eabi.lib" could not be found. So we have tried with V5.2.7 and V15.12.1.LTS which resulted in the same Problem. When I Switch back to V5.0.5 I can do a complete rebuild even after I have manually deleted the Runtime Library first.
I have read some other E2E posts addressing similar problems but without finding a solution to the problem. Some E2E Posts addressing problems that the build of the runtime library fails. But here the build does not even start.
Any help is appreciated.
Best regards,
Patrick