This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCs-Uniflash SEVERE: IcePick_C: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 6.0.83.1)



Hi

I have issues while flashing images to sensortag-cc2650

When I selected configuration I got the below error:

8<---------------------------------------------

[19:21:03] Begin Launching session operation.
[19:21:03] Cortex_M3_0: GEL Output: Memory Map Initialization Complete.

[19:21:03] ERROR >> Cortex_M3_0: Failed Board Reset

---------------------------------------------------------->8

I ignored the  above error and tried to flash the image:

the below log is seen:

8<--------------------------------------------

***** Texas Instruments Universal Flash Programmer *****

<START: 18:53:46 GMT+0530 (IST)>

> Configuring the Flash Programmer with the given configuration ...

> Flash Manager is configured for the following part: CC2650F128

> Connecting to the target for Flash operations ...

SEVERE: IcePick_C: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 6.0.83.1)

SEVERE: emulation failure occurred
SEVERE: Error connecting to the target: emulation failure occurred

------------------------------------------------------------------->8

Thanks for your help

  • Hi,

    This is an unusual error message - the only other report is mentioned in the thread below that is related to a HW problem.

    e2e.ti.com/.../484513

    I tried to "break" my Sensortag here but I was unsuccessful in getting the same error message. In this case, does the "Test Connection" button report any errors?

    One last thing I recalled - are you using the Sensortag Devpack? If so, check if the device in the Devpack is overheating and, in case affirmative, refer to the other thread below:

    e2e.ti.com/.../433497

    Hope this helps,
    Rafael