This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gents and Ladies,
My CCS 6.1.1 in Win 7 gives me the java Exception error every first time I select the Debug perspective.
This is a recent, fresh installation of CCS. The very same issue happened on 6.0 before - it's been here for over a year...
It does not prevent my from doing anything, but it is kind of annoying - particularly when using the machine to teach colleagues, who stare at you with a "can't you properly install software in your PC?" look...
Then, when closing CCS, again the same error pops up quickly before the program shuts down.
I looked into all similar errors on the forums, but they don't seem to be the same as this case.
Any hints?
Thanks
Bruno,
Is using the latest version CCS 6.2 an option for you? If so, could you give that version a try and let us know if you experience the same issue?
http://processors.wiki.ti.com/index.php/Download_CCS#Code_Composer_Studio_Version_6_Downloads
Also, FYI, the next release CCSv7 is scheduled to be released by end of the week.
If the issue is reproducible with CCS 6.2 and/or CCS 7.0, it would help us if you could generate/collect the debug server logs, Eclipse logs and dump files (as per this page) and zip them up and attach them here.
Bruno,
For the errors you refer to ( CrashTrackerJob, LicenseAcquisition and LoadingDeviceInformation) it is usually related to a corrupt or incomplete installation of Microsoft runtime libraries. Please see this page: http://processors.wiki.ti.com/index.php/Troubleshooting_CCSv6#Missing_MSVC_redistributable_libraries
The CCSv7 release will be announced tomorrow, but it is available for download today, so feel free to give it a try.
processors.wiki.ti.com/.../Category:Code_Composer_Studio_v7
I would be very interested to hear how CCSv7 works out for you.
AartiG,
Meanwhile I kept battling to apply the ~2Gb of Windows updates, and got my Win7 status all green now. After that, CCS 6.2.0 worked perfectly. The NullPointerException that originated this post no longer showed up, so it was also related to Windows components of my old installation.
Installing CCS7.0 now. One point about the installation (happened with 620 as well): it insists on telling me that it detected an anti-virus running, when there was no such. Maybe the Windows internal security or firewall? It did not prevent a good installation on 6.2.0, but the warning is debatable...
CCS7: One error during update: "can't read 'update': no such variable". The installation exited as an error. The files and directories are installed, but there is no ccstudio.exe inside DIR/eclipse/ (assuming that the structure is similar to 6.2.0).
I'll download the full version to give it a try, as the first attempt was online install. And will post on a new thread whatever happens...
Bruno
Bruno,
Bruno Saraiva said:Meanwhile I kept battling to apply the ~2Gb of Windows updates, and got my Win7 status all green now. After that, CCS 6.2.0 worked perfectly. The NullPointerException that originated this post no longer showed up, so it was also related to Windows components of my old installation.
That's great. Glad to hear that CCS 6.2 is working well now.
Bruno Saraiva said:One point about the installation (happened with 620 as well): it insists on telling me that it detected an anti-virus running, when there was no such.
Sometimes the anti-virus may still be running some processes like real-time file checking even if the AV program is disabled, and that will trigger the message. It is ok to just click through it if it does not interfere with the install process.
Bruno Saraiva said:CCS7: One error during update: "can't read 'update': no such variable".
I see that you started a new thread for this. So we will treat this thread as resolved and work the CCSv7 install issue in the other thread.
Thanks for your patience.