Hello TI,
I built the SBL for TDA3x, but I cannot find some functions in map file (sbl_qspi_opp_nom_ipu1_0_release.xem4.map).
I added FUNCTION_OPTIONS pragma, still cannot find. Any extra steps need to do?

Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI,
I built the SBL for TDA3x, but I cannot find some functions in map file (sbl_qspi_opp_nom_ipu1_0_release.xem4.map).
I added FUNCTION_OPTIONS pragma, still cannot find. Any extra steps need to do?

Thanks.
Hao,
there are some limitations with the FUNCTION_OPTIONS pragma which are described in more detail in another E2E thread (pragma FUNCTION_OPTIONS not overriding project flags). Due to these limitations it's not possible to use this pragma to disable optimization of just a single function in a file. Instead I would recommend to stay with file options for the optimization level. If reducing this level from currently used -O3 to -O2 instead, the function you're interested in will not be inlined anymore and you can find the symbol in the generated map file. I think for debugging purposes it should be ok to temporary reduce the optimization level of a file.
Best regards,
Manfred
Hello Manfred,
Thanks for your reply.
In our script, it is common to set the same options to all files, setting a separate option to specific file will need some script work instead.
It should be the same case in TI SBL build.
But I think it is acceptable.
Thanks