Part Number: TMS320F28377S
Tool/software: TI C/C++ Compiler
Hi,
I am using compiler TI v15.12.1.LTS for the F28377s, and CCS 7.0.x. I have a function containing a loop that I have hand optimized with NOPs to execute in exactly 250 clocks. So I would like to be able to modify the project's compiler optimizations while holding this function with no optimizations so my loop remains constant. However, whether I set the project to -O0 and the FUNCTION_OPTIONS pragma to
#pragma FUNCTION_OPTIONS (send_led_data, "--opt_level=3")
or vice-versa, it appears that the function send_led_data is still being compiled with the project's -Ox flag and the pragma is ignored. Perhaps I am missing some other setting to make FUNCTION_OPTIONS work?
Thanks, dave