I study about processing sound.
I use C6713 and ccs6 for it.
I made new project and add source file. The source file need some header files. In addition, each header file need other many header files.
So I add folder have the h files by connecting link.
h files are request from source file are included normally, but h files are request from the h files can't be included. Then follow error diplay.
"could not open file"
But the files exist certainly in linked folder.
I wrire "#include <h file>" in source file to request from header file.
I think that connecting link of folder is making pass to the folder. This is right??
I'm sorry to ask such a rudimentary question, but please tell me.
Kota