Other Parts Discussed in Thread: RM44L520
Hi, everyone.
Device: RM44L520, CCS v8.3.1, Compiler v18.1.8.LTS
Purpose: Options (use case for tool qualification) selection
Question:
1. Among the options defined as default in the compiler options, are the options not displayed in the flags set applied at compile time?
Example, default of --symdebug:dwarf_version is 3 by user guide, but is not specifies separately in build option, and is not displayed in "Summary of flags set".
In this case, default options is applied when compiling? (-g option is used)
The other options that not shown in the (Compiler option summary) window (e.g. --c89, --float_operations_allowed=all, --relaxed_ansi, --opt_for_speed=1, etc) operates as default value?
2. Currently, we are checking compiler options according to the ToolDefinition document for ARM CGT v18.1.8.LTS tool qualification.
I want to organize the compiler options for coverage analysis request. When sending compiler option information along with coverage files, do I need to send default option information above as well?
In addition, among the options defined in "ToolDefinition.pdf" v1.2 Table 6.2 (SAFETI-COMPILER-QUALIFICATION-KIT-1_1_2-ARM_18.1.exe),
what do the options not found in SPNU151R and SPNU118U mean? (e.g. --keep_unneeded_statics, -no_inlining, etc)
Regards.