This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
Every time i try to build any new project in Code composer studio i get this error "C:/ti/ccs1040/ccs/utils/bin/gmake" is not found in PATH ". Because of which i can't run any of my code. So please provide the permanent solution on this.
My current version is Version: 10.4.0.00006
Also i checked that the preloaded examples are also not get debugged properly same error is coming.
Please respond soon
BR
Hello,
i get this error "C:/ti/ccs1040/ccs/utils/bin/gmake" is not found in PATH ".
First thing to check is if there is a gmake.exe file in the above path. Does the file exist?
If so, please check the below troubleshooting section on gmake issues:
https://software-dl.ti.com/ccs/esd/documents/sdto_ccs_build-errors.html#ccs-gmake-errors
Thanks
ki
Thanks for the reply Ki
I checked but this file doesn't exist in this path. I am getting doubt that issue is with package that i installed or the procedure that i followed for installation.
What should be done to overcome this, please respond.
BR
Assuming you installed CCS in C:\ti\ccs1040, if gmake.exe is missing then something went wrong with the CCS installation or the file got quarantined by your antivirus software or something similar to that effect. There should be five files in C:\ti\ccs1040\ccs\utils\bin. Do you see any other files in there?
You are missing gmake.exe. I don't know why this is happening. If a reinstallation failed also, then I suspect it is your antivirus that is removing the file. I would recommend you disabling it and try reinstalling and running CCS.
I also attached the missing gmake file. I suppose you can try copying that into the directory and giving it a try. However I am concerned that you may have other missing files: