This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Headless build for cross-compile project - JVM terminated with exitcode -1

Hello,

I've problem with headless build for corss-compilation project based on CCS10 IDE.

What i want to achive:

Simply saying i want to have project which i can compile for both platforms (windows and linux) depending on the platform. It's also necessary to build it from command line.

What i have now:


I've unit-test project for production code. In general my development environment is windows, but i need to run those tests during CI/CD process too.
Our jenkins is based on ubuntu. So i created new cross-compile project and configured it for both hosts - build configurations names are windows and linux.

First i tested it from the GUI perspective and it builds well on both platforms.

Then i tried to build it from command line and i occured strange issue.

Namely when i start headless build under linux, project compiles without erros, but JVM exits with exitcode -1.

It looks like it's looking for mingw32-gcc/mingw32-g++ somewhere on PATH. But minGW is configured only for windows build configuration.


Here is command that i use for headless build:

sudo /opt/ti/ccs1040/ccs/eclipse/eclipse -nosplash -data . -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import "project_path" -cleanBuild "project_name/linux" -printErrorMarkers

From logs i can see that build finished with no errors:


10:12:18 Build Finished. 0 errors, 0 warnings. (took 6s.749ms)

Binary is valid and i can run it without problems.

Here is what i get after added -printErrorMarkers


Headless build encountered errors
Marker [on: /bokita_sanpin_fw_unit_tests, id: 54, type: org.eclipse.cdt.managedbuilder.core.scanner.discovery.problem, attributes: [location: Project Properties, C++ Preprocessor Include.../Providers, [CDT Cross GCC Built-in Compiler Settings] options, message: Program "mingw32-gcc" not found in PATH, provider: org.eclipse.cdt.build.crossgcc.CrossGCCBuiltinSpecsDetector, severity: 2], created: 12/16/21 10:12 AM]
Marker [on: /bokita_sanpin_fw_unit_tests, id: 55, type: org.eclipse.cdt.managedbuilder.core.scanner.discovery.problem, attributes: [location: Project Properties, C++ Preprocessor Include.../Providers, [CDT Cross GCC Built-in Compiler Settings] options, message: Program "mingw32-g++" not found in PATH, provider: org.eclipse.cdt.build.crossgcc.CrossGCCBuiltinSpecsDetector, severity: 2], created: 12/16/21 10:12 AM]

Here is the JVM error:



I looked where the printErrorMarker output points to, but i didn't see any references to minGW.


Do you have any ideas what can be wrong?

Regrads,
mf

  • Hello,

    I assume you are working with a standard Eclipse CDT Managed Makre project. We do not officially support these types of project in CCS (it is not tested), though it should work. It sounds like some CDT issue. If you can share the two .*project files in the your project, I can investigate further.

    Thanks

    ki