This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have met the same problem as cashed (with Exit Code = -1073741819) in CCSV4 when I add a big loop in my C program. However, if I remove those loop lines, this problem will not occur.
Is that because some limitation of using memory?
Thanks
Chengwei
That error message is a very generic one. It can be caused by a variety of reasons. Did you crash generate a dump file (see the earlier posts in this thread)? When did you get the crash? When debugging?
Thanks
ki
note: this thread was split from: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/35980.aspx but the split was not fully successful
The answer for this thread is still in the original thread
See post by Chengwei.