This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6657: No examples found/CCS project creation

Part Number: TMDSEVM6657
Other Parts Discussed in Thread: TMS320F28388D, TMS320C6657, TMS320C6748

Hi Experts,

Good day.

Customer is using the TMDSEVM6657 board and installed the ff:

  • CCS11
  • SDK plug-in
  • Install the package of the C6000 & C66

However as per them, there is no examples found.

From this LINK in section 9.1 previous CCS version, it has the example of C6657 DSP processor. They found example in CCS11 for C2000 DSP (tms320f28388D example).

Now they are working with TMS320C6657 / TMS320C6748 for testing the FFT functions.

Questions:
It is possible to create project with one of this DSP processor in CCS11 with specific library? Or they need to install previous version? 9? or 10?

Thank you.

Regards,
Archie A.