This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CCSTUDIO-SITARA
I'm implementing IPC code to communicate between the A3 core running Linux and a R5 core with no RTOS. I've copied the code samples on file:///C:/TI/mcu_plus_sdk_am64x_08_01_00_36/docs/api_guide_am64x/DRIVERS_IPC_RPMESSAGE_PAGE.html, to use as a guide, as well as using the SysCfg tool.
Everything builds correctly, but I recieve the following warning:
#10247-D creating output section ".resource_table" without a SECTIONS specification fdic C/C++ Problem
I've seen references to this problem when dealing with the PRU, but that doesn't appear to apply here. My linker.cmd file appears to match the file in the sdk example, except for a couple of address differences.
Any suggestions would be appreciated. Thanks.
Lee Thalblum
Hi Lee,
Did you add the .resource_table to your linker.cmd file? Please refer to the linker.cmd files in "ipc_rpmsg_echo_linux" example. Here is the section in file:///C:/TI/mcu_plus_sdk_am64x_08_01_00_36/docs/api_guide_am64x/DRIVERS_IPC_RPMESSAGE_PAGE.html:
------------------------
.resource_table
MUST be placed in the SECTIONS
field in the linker command file at an alignment of 4K bytes.------------------------
Best regards,
Ming