This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5.0 - fatal error: could not open source file "xdc/std.h"

I have just installed Code Composer v5.0.2 and imported a project that I've been using with v4.  I'm getting an error: fatal error: could not open source file "xdc/std.h".  I am including <xdc/std.h> in my main.h file.  In the build properties for the project, I do have C:\Program Files (x86)\Texas Instruments\ccsv5\xdctools_3_20_08_88\packages\xdc as listed, which is where the std.h file is located.  Also, if I ctl-click on the <xdc/std.h> in main.h, then the std.h file is displayed, so it seems like the build tools should be able to find the file.  How do I let the compiler know the location of this file?

  • What happens if you add "C:\Program Files (x86)\Texas Instruments\ccsv5\xdctools_3_20_08_88\packages" to your include paths.  i.e. without the \xdc

  • Well, it still doesn't compile, but I do get a different error:

    "C:/Program Files (x86)/Texas Instruments/ccsv5/xdctools_3_20_08_88/packages/xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...

  • I am getting same errors from project imported from ccs v3.

     

  • I can see the same thing when creating a BIOS6 project in v4 and importing into v5.

     

    When I look at the console it shows some odd feedback at the beginning that makes it seem like one of the build tools is being called with the wrong parameters.  Let me look into this.

     

    Usage: xs xdc.tools.configuro [--help]

    [-v | -q]

    [-@ optionsfile]

    [-o outdir]

    [-b config_bld | -c codegen_dir | --cb]

    [-t target] [-p platform[:instance]] [-r profile]

    [-Dname=value]

    [-w | -x regexp]

    [--rtsName pkg_name]

    [--cfgArgs args_string]

    [--linkTemplate linker_template]

    [--tcf] [--bios5] [--pkg] [--generationOnly]

    [--compileOptions compile_options_string]

    [--oc compiler.opt] [--ol linker.cmd]

    infile.cfg

    'Finished building: ../hello.cfg'

  • have you had any luck getting to the problem?

  • Evan,

    I heard back from the dev team today.  The problem is coming about because the project system in 4.2.2/3 is in some ways "newer" than what is in 5.0.2/3.  i.e. the 4.x stream is still evolving.  The problem doesn't exist when importing into CCSv5.1.

    So an option is to move to CCSv5.1.  It is not a production tool yet but it is available.  Is that something you would want to pursue?

    Regards,

    John

  • sure, I'm happy to give that a try.

  • You can get the 5.1 M4 build here http://processors.wiki.ti.com/index.php/Category:Code_Composer_Studio_v5

    We are doing monthly milestone builds for 5.1 so there will be another build in 2-3 weeks.

     

    John

  • awesome, this version built and ran my projects with no issues.

  • Hi Johns

    I have similiar issue of importing ccs4.2.3 to ccs5.0.3 as the attached  building log (fftcTest.build.log) after I directly added the rtsc path into the include option for compiling. I also created a hello RTSC example pjt  from the wizrad and got the same compiling error.  Well there woll be no compiling error if I choose custom c6000 device but not generic c66x from the CCS build ->general option, but in this case, instead I got linking error as the attached log hello.build.log.

    Altough ccs5.1 can get this issue resolved, could you provide any workground for ccs 5.0 too if there is any? (I got suggested that ccs 5.0.3 is a better choice since ccs5.1 may not be so stable as it should be currently)

    BTW: could I have any suggestions on how to stop the disgusting "refresh workspace"in the building process which slows the whole comping progress greatly(I can't manually stop it once fo

    **** Build of configuration Debug for project fftcTest ****
    
    C:\Program Files\Texas Instruments\ccsv5\utils\gmake\gmake -k all 
    'Building file: ../fftcTest.cfg'
    'Invoking: XDCtools'
    "C:/Program Files/Texas Instruments/xdctools_3_20_08_88/xs" --xdcpath="C:/Program Files/Texas Instruments/bios_6_31_04_27/packages;X:\4gbts_msp\Platform\Export\packages\npc\platforms;C:/Program Files/Texas Instruments/xdais_7_20_00_07/packages;C:/Program Files/Texas Instruments/xdais_7_20_00_07/examples;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66_big_endian -p TCI6616_BBU -r whole_program -c "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000" -Dconfig.importPath=X:/4gbts_msp/Platform/Export\configuration TCI6616_BBU "../fftcTest.cfg"
    Usage: xs xdc.tools.configuro [--help]
    	[-v | -q]
    	[-@ optionsfile]
    	[-o outdir]
    	[-b config_bld | -c codegen_dir | --cb]
    	[-t target] [-p platform[:instance]] [-r profile]
    'Finished building: ../fftcTest.cfg'
    	[-Dname=value]
    ' '
    'Building file: ../MSP_BuildEnvironment.cpp'
    	[-w | -x regexp]
    	[--rtsName pkg_name]
    	[--cfgArgs args_string]
    	[--linkTemplate linker_template]
    	[--tcf] [--bios5] [--pkg] [--generationOnly]
    	[--compileOptions compile_options_string]
    	[--oc compiler.opt] [--ol linker.cmd]
    	infile.cfg
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_BuildEnvironment.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_BuildEnvironment.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    
    >> Compilation failure
    1 fatal error detected in the compilation of "../MSP_BuildEnvironment.cpp".
    Compilation terminated.
    gmake: *** [MSP_BuildEnvironment.obj] Error 1
    'Building file: ../MSP_CpintcSetup.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_CpintcSetup.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_CpintcSetup.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_CpintcSetup.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_CpintcSetup.obj] Error 1
    'Building file: ../MSP_EdmaDefaultConfig.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_EdmaDefaultConfig.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_EdmaDefaultConfig.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_EdmaDefaultConfig.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_EdmaDefaultConfig.obj] Error 1
    'Building file: ../MSP_EdmaInterrupt.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_EdmaInterrupt.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_EdmaInterrupt.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_EdmaInterrupt.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_EdmaInterrupt.obj] Error 1
    
    (Command canceled)
    r ever)?


    Thanks very much!

    BR/Gavin

    **** Build of configuration Debug for project hello ****
    
    C:\Program Files\Texas Instruments\ccsv5\utils\gmake\gmake -k all 
    'Building file: ../hello.cfg'
    'Invoking: XDCtools'
    "C:/Program Files/Texas Instruments/xdctools_3_20_08_88/xs" --xdcpath="C:/Program Files/Texas Instruments/bios_6_31_04_27/packages;C:/Program Files/Texas Instruments/ipc_1_22_03_23/packages;X:\4gbts_msp\Platform\Export\packages\npc\platforms;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66_big_endian -p TCI6616_BBU -r whole_program -c "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000" "../hello.cfg"
    making package.mak (because of package.bld) ...
    generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
    configuring hello.pe66e from package/cfg/hello_pe66e.cfg ...
    cle66e package/cfg/hello_pe66e.c ...
    lnke66e hello.pe66e ...
    'Finished building: ../hello.cfg'
    ' '
    'Building target: hello.out'
    'Invoking: C6000 Linker'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --diag_warning=225 --big_endian --abi=eabi -z -m"hello.map" --warn_sections -i"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/lib" -i"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --reread_libs --rom_model -o "hello.out" -l"./configPkg/linker.cmd"  "./hello.obj" 
    <Linking>
    
     undefined             first referenced                                                                                             
      symbol                   in file                                                                                                  
     ---------             ----------------                                                                                             
     HOSTwrite             D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     __TI_decompress_none                                                                                                               
     __TI_decompress_rle24                                                                                                              
     __TI_zero_init                                                                                                                     
     __c6xabi_divlli       D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     __c6xabi_divu         D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     __c6xabi_remu         D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     _args_main            C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\ti\targets\rts6000\lib\boot.ae66e<boot.oe66e>
     _nop                  D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     _register_lock        D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     _register_unlock      D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     abort                 D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     atexit                D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     exit                  D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     memcpy                D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
     memset                D:/Work/TI/CCS5/hello/Debug/configPkg/package/cfg/hello.pe66e.obj                                            
    
    error: unresolved symbols remain
    error: errors encountered during linking; "hello.out" not built
    
    >> Compilation failure
    gmake: *** [hello.out] Error 1
    gmake: Target `all' not remade because of errors.
    

    **** Build of configuration Debug for project fftcTest ****
    
    C:\Program Files\Texas Instruments\ccsv5\utils\gmake\gmake -k all 
    'Building file: ../fftcTest.cfg'
    'Invoking: XDCtools'
    "C:/Program Files/Texas Instruments/xdctools_3_20_08_88/xs" --xdcpath="C:/Program Files/Texas Instruments/bios_6_31_04_27/packages;X:\4gbts_msp\Platform\Export\packages\npc\platforms;C:/Program Files/Texas Instruments/xdais_7_20_00_07/packages;C:/Program Files/Texas Instruments/xdais_7_20_00_07/examples;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66_big_endian -p TCI6616_BBU -r whole_program -c "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000" -Dconfig.importPath=X:/4gbts_msp/Platform/Export\configuration TCI6616_BBU "../fftcTest.cfg"
    Usage: xs xdc.tools.configuro [--help]
    	[-v | -q]
    	[-@ optionsfile]
    	[-o outdir]
    	[-b config_bld | -c codegen_dir | --cb]
    	[-t target] [-p platform[:instance]] [-r profile]
    'Finished building: ../fftcTest.cfg'
    	[-Dname=value]
    ' '
    'Building file: ../MSP_BuildEnvironment.cpp'
    	[-w | -x regexp]
    	[--rtsName pkg_name]
    	[--cfgArgs args_string]
    	[--linkTemplate linker_template]
    	[--tcf] [--bios5] [--pkg] [--generationOnly]
    	[--compileOptions compile_options_string]
    	[--oc compiler.opt] [--ol linker.cmd]
    	infile.cfg
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_BuildEnvironment.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_BuildEnvironment.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    
    >> Compilation failure
    1 fatal error detected in the compilation of "../MSP_BuildEnvironment.cpp".
    Compilation terminated.
    gmake: *** [MSP_BuildEnvironment.obj] Error 1
    'Building file: ../MSP_CpintcSetup.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_CpintcSetup.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_CpintcSetup.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_CpintcSetup.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_CpintcSetup.obj] Error 1
    'Building file: ../MSP_EdmaDefaultConfig.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_EdmaDefaultConfig.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_EdmaDefaultConfig.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_EdmaDefaultConfig.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_EdmaDefaultConfig.obj] Error 1
    'Building file: ../MSP_EdmaInterrupt.cpp'
    'Invoking: C6000 Compiler'
    "C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --include_path="C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --include_path="C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages" --include_path="X:/4gbts_msp/platform/CcsProjects" --include_path="X:/4gbts_msp/Platform/Components/FFTc/TestHarness/srcGen/src" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages" --include_path="X:/4gbts_msp/Platform/Components/utilities/lib/Nyquist/v1.0.0.21/packages/ti/csl" --include_path="X:/4gbts_msp/Platform/Components/utilities/h" --include_path="X:/4gbts_msp/Platform/Components/FFTc/testVector" --include_path="X:/4gbts_msp/Platform/Export/include" --diag_warning=225 --big_endian --mem_model:const=far --mem_model:data=far --abi=eabi --preproc_with_compile --preproc_dependency="MSP_EdmaInterrupt.pp" --cmd_file="./configPkg/compiler.opt"  "../MSP_EdmaInterrupt.cpp"
    >> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
    "C:\Program Files\Texas Instruments\xdctools_3_20_08_88\packages\xdc/std.h", line 76: fatal error: #error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
    1 fatal error detected in the compilation of "../MSP_EdmaInterrupt.cpp".
    Compilation terminated.
    
    >> Compilation failure
    gmake: *** [MSP_EdmaInterrupt.obj] Error 1
    
    (Command canceled)

  • Gavin,

     'xdc_target_types__' must be defined to name a target-specific header file (e.g., ti/targets/std.h) that has definitions for the basic types:

     xdc_Int8, xdc_Int16, ...

     For example, to build for a target in the ti.targets package you should

     add the following option to your compiler's command line:

     -D xdc_target_types__=ti/targets/std.h

    If you have set the include paths correctly and if you define the above you will not see the error in CCS 5.0

    Please try this and let us know if this resolves your error.

     

    Regards,

    Rahul

     

     

  • I have code composer  Version: 5.1.0.09000 and have been trying to get the uart_echo example project compiled on my system.  I get the compile error:

    D:\ti\ccsv5\utils\bin\gmake -k all
    'Building file: C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/startup_ccs.c'
    'Invoking: TMS470 Compiler'
    "D:/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7M3 -g -O2 --gcc --define=ccs --define=PART_LM3S9B92 --define=TARGET_IS_TEMPEST_RB1 --include_path="D:/ti/ccsv5/tools/compiler/tms470/include" --include_path="C:/projects/9200/uart_echo/inc" --include_path="C:/projects/9200/uart_echo/../StellarisWare/inc" --include_path="C:/projects/9200/uart_echo/../../../.." --include_path="C:/projects/9200/uart_echo" --include_path="c:/StellarisWare/" --diag_warning=225 -me --gen_func_subsections --abi=eabi --code_state=16 --ual --preproc_with_compile --preproc_dependency="startup_ccs.pp"  "C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/startup_ccs.c"
    'Finished building: C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/startup_ccs.c'
    ' '
    'Building file: C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/uart_echo.c'
    'Invoking: TMS470 Compiler'
    "D:/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7M3 -g -O2 --gcc --define=ccs --define=PART_LM3S9B92 --define=TARGET_IS_TEMPEST_RB1 --include_path="D:/ti/ccsv5/tools/compiler/tms470/include" --include_path="c:StellarisWare/" --include_path="C:/projects/9200/uart_echo/../../../.." --diag_warning=225 -me --gen_func_subsections --abi=eabi --code_state=16 --ual --preproc_with_compile --preproc_dependency="uart_echo.pp"  "C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/uart_echo.c"
    "C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/uart_echo.c", line 26: fatal error: could not open source file "inc/hw_memmap.h"
    1 fatal error detected in the compilation of "C:/StellarisWare/boards/ek-lm3s9b92/uart_echo/uart_echo.c".
    Compilation terminated.

    I have tried adding all kinds of include formats in every syntax I can think of to try to get it able to see the file hw_memmap.h and have copied the file into other directories - but none of it works.  At the time I imported this project, I remember getting some errors.  I though it would be easier to get one of the example projects for EKK-LM3S9B92 evaluation kit to compile and run.

    Eric Krieg