Other Parts Discussed in Thread: TMS320F28388D, TMS320F28335
Hi,
CCS : v11.1.0.00011
CGT : C2000 TI v21.6.0.LTS
Processor : TMS320F28388D
Area where the code runs : Internal RAM
I've a problem with setting a breakpoint on a specific line or code in the source file.
If I select a code or line by dragging the mouse and set a breakpoint through the shortcut menu by clicking the right mouse button, the breakpoint is not set normally.
However, if I set a breakpoint by calling the shortcut menu with the right mouse button in the Breakpoints tab and directly entering the address of a specific code, I can set the breakpoint normally.
I wonder what is causing this problem.
(Please refer to the video attached to this post.)
Thanks.