I can set a breakpoint in my GEL files using GEL_HWBreakPtAdd("<function>");
I can set a breakpoint inside a function by right-clicking on the line.
I have not found a way to set a breakpoint on a line or a label using a GEL function.
Is this possible?
I have tried
GEL_HWBreakPtAdd("mysource.c:78");
GEL_HWBreakPtAdd("mysource.c, line 78");
GEL_HWBreakPtAdd("mysource.c", 78);
but neither is consider a valid breakpoint.
Is is possible, if paths are added?