Hi,
below is the last part of the installation log on win10 21H2 x64. Please, let me know if the issue is know, and if there is a workaround for the error.
Best Regards, Andrei
-------- installation log --------
Unpacking files
Unpacking C:\ti\ccs1210\ccs\ccs_base\DebugServer\drivers\TI_Bug_Icon_Red.ico
Executing C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF\installCerts.bat
Script exit code: 0
Script output:
Script stderr:
Executing C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF"
Script exit code: unknown signal
Script output:
Script stderr:
child killed: unknown signal
Error running C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF": child killed: unknown signal
[11:35:32] dpinst return code = unknown signal
Exiting with code -1