This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
below is the last part of the installation log on win10 21H2 x64. Please, let me know if the issue is know, and if there is a workaround for the error.
Best Regards, Andrei
-------- installation log --------
Unpacking files
Unpacking C:\ti\ccs1210\ccs\ccs_base\DebugServer\drivers\TI_Bug_Icon_Red.ico
Executing C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF\installCerts.bat
Script exit code: 0
Script output:
Script stderr:
Executing C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF"
Script exit code: unknown signal
Script output:
Script stderr:
child killed: unknown signal
Error running C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\ccs1210/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF": child killed: unknown signal
[11:35:32] dpinst return code = unknown signal
Exiting with code -1