This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28388S CCS 12.3.0 error

Description Resource Path Location Type
#10010 errors encountered during linking; "28377S_ANPC.out" not built 28377S_ANPC C/C++ Problem


Description Resource Path Location Type
#16041-D File "../rts2800_fpu32_eabi.lib<s_ceil.c.obj>" passes/returns double types in memory while previous files pass them in {3} 28377S_ANPC C/C++ Problem

Description Resource Path Location Type
gmake: *** [all] Error 2 28377S_ANPC C/C++ Problem

Description Resource Path Location Type
gmake[1]: *** [28377S_ANPC.out] Error 1 28377S_ANPC C/C++ Problem

error #16041-D: File "../rts2800_fpu32_eabi.lib<s_ceil.c.obj>" passes/returns double types in memory while previous files pass them in {3}
error #10010: errors encountered during linking; "28377S_ANPC.out" not built

gmake[1]: *** [28377S_ANPC.out] Error 1

gmake: *** [all] Error 2

I don't understand this error..

help please.

and I want know DSP 28388S stand by alone mode....

I think flash boot mode... 

I want how to DSP 28388stand by alone mod... 

Can you help me?,,,

Thank you!

  • Hello,

    I have brought this thread to the attention of the compiler experts. Please note that due to the local holiday it may take until Wednesday for a response. 

    Thank you for your paitence.

    ki

  • Please rebuild the entire project.  One way to do that is to right-click on the name of the project and select Rebuild Project.  Then save the contents of the Console (not Problems) view to a text file.  Use the icon named Copy Build Log.  When you name the log file, be sure to use the file extension .txt.  Please attach that text file to your next post.

    Thanks and regards,

    -George