Part Number: CODECOMPOSER
1.Test connection in linux(Virtualbox ubuntu22) always have following log:
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: E_RPCENV_IO_ERROR(-6)
Download failed for file /home/lxxm/ti/ccs1230/ccs/ccs_base/common/uscif/./xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
2.But in windows,it connect successfully.