Other Parts Discussed in Thread: CODECOMPOSER
Hi,
I have two questions.
1) Does the target get reflashed every time the debugger is connected or only if the downloaded image has been changed?
2) How do I get the debugger to display the value of static variables?
for instance in the block below from main_AP.c in eZ430-RF2500 example code, if I set a breakpoint on
(SMPL_SUCCESS == SMPL_Receive(sLID[i], msg, &len))
the debugger stops OK but I cannot read either the value of the local variable i or or the static sNumCurrentPeer, although other variables are displayed OK.
if
(sPeerFrameSem)
{
uint8_t msg[MAX_APP_PAYLOAD], len, i;
/* process all frames waiting */
(i=0; i<sNumCurrentPeers; ++i)
{
if
(SMPL_SUCCESS == SMPL_Receive(sLID[i], msg, &len))
Thanks in advance for any help,
John.