Hi,
I'm running mcu_plus_sdk_243x Hello.cpp example.
Is it possible to set breakpoints before the main() function? ( To see static variables initialization)
Thanks,
Eli
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm running mcu_plus_sdk_243x Hello.cpp example.
Is it possible to set breakpoints before the main() function? ( To see static variables initialization)
Thanks,
Eli
Hi,
I found some entry point for main function

but I don't know what to put instead of main - to view all global objects initialization
For example I put before main()
MyObjectPtr* = new CMyClass();
I would like to debug the code that does the new (all the memory allocations)
Thanks,
Eli
You probably need to break into cinit, the source should be available, but it might not be compiled with debugging symbols;
You are getting beyond my ken - especially with C++ - but in startup_msp432P401r_ccs.c there is this:
/* Forward declaration of the default fault handlers. */
/* This is the code that gets called when the processor first starts execution */
/* following a reset event. Only the absolutely necessary set is performed, */
/* after which the application supplied entry() routine is called. Any fancy */
/* actions (such as making decisions based on the reset cause register, and */
/* resetting the bits in that register) are left solely in the hands of the */
/* application. */
void Reset_Handler(void)
{
SystemInit();
/* Jump to the CCS C Initialization Routine. */
__asm(" .global _c_int00\n"
" b.w _c_int00");
}
Hi,
Yes but when I put the entry to _c_int00 and single step from there - I'm not getting to global C++ initialization just to the BSS.
I see all kind of entries at boot_armv7r.c - but which to choose ?
Thanks,
Eli
Hi,
You can disable the run to main option then your code won't run till main and you can put breakpoint post that.
Regards,
Ankur