Other Parts Discussed in Thread: TMS320F28035
Hello Ti Team.
I have a problem with XDS560 v2 Blackhawk JTAG emulator (TMDSEMU560V2STM-EU). When I trying to Test Connection from CCS Target Configuration window I get these errors:
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\xxx\AppData\Local\TEXASI~1\CCS\
ccs1240\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
Loaded FPGA Image: C:\ti\ccs1240\ccs\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Sep 6 2023'.
The library build time was '14:41:42'.
The library package version is '9.13.0.00201'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-100' (0xffffff9c).
The title is 'SC_ERR_BAD_GENERIC'.
The explanation is:
The controller or software detected an error with an unknown cause.
This error number is used when detailed information is not available.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
No matter how it is connected (via USB or LAN) error message is the same. I connecting it to the board with TMS320F28035 MCU on it.
EDIT:
When I run all tests from Blackhawk XDS560v2 Configuration Utility v 1.0.0.14 I have these messages:
CMD: dbgjtag -X emulator,driver=bh560v2e,ioport=0xc0a8d40a -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000 Loaded FPGA Image: c:\ti\ccs1240\ccs\ccs_base\common\uscif\dtc_top.jbc An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-286' (0xfffffee2). The title is 'SC_ERR_CLK_PLL_HUNG'. The explanation is: The PLL programming function has suffered a timeout. This may be an honest-to-goodness software or VHDL bug. RES: dbgjtag -X emulator,driver=bh560v2e,ioport=0xc0a8d40a -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000 RES: Fail