This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

blackhawk connection



Hi,

I use the TMDXEVM6678LE, now I have a problem when I connect to the board.

When I power on the EVM, the green LED(D3) turns on. Then the yellow LED(D2) and red LED(D1) should turn on.

But now only red LED turns on. It is not in safe mode.

When I test the connection, the output is as follows:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\ADMINI~1\AppData\Local\.TI\213602635\
0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
The library build date was 'May 30 2012'.
The library build time was '23:17:26'.
The library package version is '5.0.747.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-100' (0xffffff9c).
The title is 'SC_ERR_BAD_GENERIC'.

The explanation is:
The controller or software detected an error with an unknown cause.
This error number is used when detailed information is not available.

[End]

So, what should I do?

Why does this phenomenon occur?

Thanks.