Hi,
I just updated CCS from v4.2.1 to v4.2.4. Also, updated to latest CGT, Spectrum Digital updates, etc.
I initiated the update through Help-->Software-->Find and Install
After the update was finished I couldn't build any of the existing projects. I got the following message:
"This project was created for a device-variant that is not currently recognized: TMS320C55XX.TMS320VC5515. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants. "
When I tried to go into CCS Build in Project Properties I got the following message: "The currently displayed page contains invalid values".
Any idea how to solve this without a complete uninstall of CCS (I don't want to have to separately download the full image of CCS 4.2.4 or downgrade to a version that clearly has problems) ?
Thanks,
Shahar